AXIS#.FBUS.PROTECTION

Description

When an AKD2G is a slave node on a fieldbus (for example an AKD2G is connected to an EtherCAT master) and WorkBench is simultaneously connected to an AKD2G using a service channel, there are several options for the AKD2G to respond to commands from each of the channels.

When the fieldbus is operational, the AKD2G uses the AXIS#.FBUS.PROTECTION parameter to select how commands from WorkBench, or any other device sending commands to the drive through a service channel, should be handled. WorkBench uses either of two service channels: Telnet or ASCII SDO. Both service channels are affected identically by AXIS#.FBUS.PROTECTION.

The following table shows the available options. If the fieldbus is not connected or not started, then parameters executed through a service channel are not blocked.

Value Description
0 Motion and Tuning Commands Allowed - Commands that interfere with motion are allowed. Gain and IO configuration changes are allowed.

DRV.HELP includes the [Blocked] attribute to indicate if a parameter is being blocked. For example, if AXIS#.FBUS.PROTECTION is 0 and the network is operational, the following help is shown.

-->DRV.HELP AXIS1.EN
Help for: AXIS1.EN [ActionCommand] [Blocked]
-->

If an attempt is made to execute a blocked parameter, the following error appears.

-->AXIS1.EN
Error: [0106] Command blocked while fieldbus is operational.

All write or command functions of a parameter are blocked by AXIS#.FBUS.PROTECTION. AXIS#.FBUS.PROTECTION does not block the read function of any parameter.

If a parameter is blocked through telnet, it is accessible through the fieldbus. For example, SDOs in the case of CANopen or EtherCAT.

Use AXIS#.FBUS.BLOCKING to read if the axis is blocked.

Parameters Affected by AXIS#.FBUS.PROTECTION

This is a list of all parameters that are blocked when AXIS#.FBUS.PROTECTION is 1 and CANOPEN.STATE = 5 (operational).

  • AXIS#.EN
  • AXIS#.DIS
  • AXIS#.OPMODE
  • AXIS#.CMDSOURCE
  • AXIS#.STOP
  • AXIS#.CLRFAULTS
  • DRV.CLRFAULTS
  • AXIS#.SM.MOVE
  • AXIS#.MT.MOVE
  • AXIS#.HOME.MOVE
  • AXIS#.IL.CMDU
  • AXIS#.VL.CMDU
  • AXIS#.MOTOR.BRAKECONTROL

The action table and any associated active actions still operate when AXIS#.FBUS.PROTECTION is set (see Action Table).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

Not supported on analog drive models.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.FBUS.PROTECTION

5005h

01h

Unsigned8

-

-

Read/Write

No

AXIS2.FBUS.PROTECTION

5105h

01h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.FBUS.PROTECTION

5102

13EE

Unsigned8

Read/Write

-

AXIS2.FBUS.PROTECTION

70638

113E

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FBUS.PROTECTION

5102

Unsigned8

Read/Write

-